Viewing a Broadcast Management (BBMD) Object - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

To view a Broadcast Management object, complete the following steps:

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. Under the Device Information folder, click BBMD. Information about the object appears in the right section of the screen.
  4. Click View to view the BM Addresses screen. This screen provides the IP Address, UDP Port and UDP Broadcast Mask of a BM Address.
  5. Click Details in the BM Addresses screen to view individual BM Address details.