Setting up Intrinsic Alarms - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. In the Advanced Object tree, click Intrinsic Alarming. Three tabs appear in the Intrinsic Alarming dialog box:
    Note: Click the columns to sort the information in these tabs.
  4. Click the tab you want and click Edit. The fields that you can edit appear in white.
  5. To turn on intrinsic alarming for a point, click True in the Intrinsic Alarming field for the point you want. When you set a point’s Intrinsic Alarming field to True, the system allows you to edit the alarm attributes for the point.
  6. Edit the remaining alarm attributes for the point and click Apply.