Setting up Event Log Parameters - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab. The Advanced Object tree and information screen appear.
  3. In the Advanced Object tree under Intrinsic Alarming, click Event Log and then click the Details tab.
  4. Click Edit. The fields you can edit appear in white.
  5. Edit the parameters of the notification. See Event Log.