Adding a Weekly Schedule - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

Weekly schedules allow you to select the time frame for the days in your schedule.

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. In the Advanced Object tree, right-click Schedules and then click Add Schedule. A new schedule is added to the Advanced Object tree.
  4. Click the schedule located below Schedules in the Advanced Object tree.
  5. Click Edit. The fields you can edit appear in white.
  6. Enter the basic parameters. See Schedule Details Screen.
  7. In the Display Mode list, click Weekly Schedule.
  8. Click the + button. The Define New Events screen appears.
    Note: You may need to resize the screen for a better view of the Advanced tab information.
  9. Define the parameters of the weekly schedule. See Define New Events Screen.
  10. Click OK.
  11. Click Apply.