Editing Device Information - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

To edit Device Information, complete the following steps:

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab. The Device Information folder and information screen appear.
  3. Under the Device Information folder, select the controller you want to view. Information about the controller appears in the right section of the screen.
  4. Click Edit. The fields that you can edit appear in white.
  5. Edit the parameters of the device. See Device Information Screen.
  6. Click Apply.