Define New Events Screen - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See Adding a Weekly Schedule.

Table 1. Define New Events Screen

Field

Description

Monday - Sunday

Use to select the days of the week for a schedule.

Mon-Fri

Use to select Monday through Friday for a schedule.

All

Use to select all days of the week.

Hour, Minutes

Indicates the time of the day you want to schedule.

Value

Indicates the default value that appears (for example, on or occupied) for the time frame you select. For example, yellow can indicate On, and blue can indicate Off.

OK

Saves changes to the information in the screen.

Cancel

Exits the screen without saving changes

Opens the Help system.