Broadcast Management (BBMD) Object Screen - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

For information on how to view, edit, and add a Broadcast Management object, see Working with a Broadcast Management (BBMD) Object.

Table 1. Broadcast Management Object (BBMD) Screen

Field

Description

Object

Name

Indicates the name of the Broadcast Management object.

Description

Provides a basic description of the Broadcast Management object.

Object Identifier

Indicates the BACnet object ID for the Broadcast Management object.

Enabled

Select True or False to disable or enable BBMD functionality. This selection can be configured in the Transfer Summary screen. See Transfer to Device (Download).
Note: Enable only one device as a BBMD on a given subnet. If you do not know how to configure a BBMD, do not enable BBMD in your application or device. For further information, refer to the Metasys IP Networks for BACnet/IP Controllers Configuration Guide Technical Bulletin (LIT-12012468) .
Network

BM Address List

Use this attribute to configure the endpoints that communicate with the BBMD. To view or edit this list see Viewing a Broadcast Management (BBMD) Object and Editing a Broadcast Management (BBMD) Object.

Broadcast Disabled

Indicates the broadcast status.