Making a ZigBee Connection - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. Open the tool.
  2. Click the Commission button. The Commission Device Wizard appears.
  3. Make your application transfer type and ZigBee connection type selections.
  4. Enter your connection parameters, choose your Product Type, and click Next.
  5. Select the device and click Next. The Commission Device Summary dialog box appears.
    Note: If you have selected Current Application, only the Field Device defined in your CAF appears in the selection list.