Making a MAP 4.2+/BACnet Router Connection - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. Open the tool.
  2. Click Commission. The Commission Device Wizard appears.
  3. Select application and connection attributes, then click Next.
  4. Select the device and click Next. The Commission Device Summary dialog box appears.
    Notes:
    • If you have selected Current Application, only the Field Device defined in your CAF appears in the selection list.
    • Do not use 1001 for the MS/TP Network Number. The MS/TP Network Number 1001 is reserved for Johnson Controls IP network connections.