Making a Bluetooth Connection - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Procedure

  1. Open the tool.
  2. Click Commission. The Commission Device Wizard appears.
  3. Select the application transfer type and Bluetooth connection type.
  4. Enter your connection parameters, choose your Product Type, and click Next.
  5. Select the device and click Next. The Commission Device Summary dialog box appears.
    Note: If you have selected Current Application, only the Field Device defined in your CAF appears in the selection list.