Modifying Offsets - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. Right-click an input or miscellaneous input and select View Details. The Details dialog box appears.
  2. Click Edit.
    Note: When in Edit mode the system stops polling data until the window closes. System data polling immediately resumes when the dialog box is closed.
  3. Enter the desired offset value.
  4. Click OK.