For information on showing and hiding involvement, see Showing and Hiding Involvement. When you view this dialog box, the magenta highlighting indicates which modules are affecting the selected output.
| Field | Description |
|---|---|
| Network Inputs | List of network inputs. |
| Inputs | List of inputs. |
| Miscellaneous Inputs | List of miscellaneous inputs. |
| Setpoint/Miscellaneous | List of setpoint miscellaneous modules. |
| State Generation | List of state generation modules. |
| Output Control | List of output control modules. |
| Network Outputs | List of network outputs. |
| Outputs | List of outputs. |
| Miscellaneous Outputs | List of miscellaneous outputs. |
|
|
Opens the Help system. |
| Close | Closes the dialog box. |