FSM Details Screen - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
Table 1. FSM Screen (Commissioning Mode)
Field Description
Realtime Display

Locks FSM to the current state of the running application.

Manually Browse

Enables the user to explore all potential states of an application.

Current State

Current state.

Previous State

Previous state. 1

Time in State

Indicates the length of time in the current state.1

Possible Next States

Possible next states for the current state.

State Name

State name.

Guard Condition

Conditions which must be true in order to transition to the next state.

Note: At Release Mode 10.4 / Firmware 8.0, if any part of a guard condition is True, it will be highlighted in green and bold text.
1 This feature is only available in Release Mode 10.4 / Firmware 8.0.