Flow Restore Command Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1. Flow Restore Command Dialog Box

Field

Description

Do you want to send Flow Restore Command?

Send

Issues the Flow Restore command.

Cancel

Closes the dialog box without issuing the command.