Flow Override Command Dialog Box - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
Table 1. Flow Override Command Dialog Box

Field

Description

Attribute

Attribute being commanded. You cannot edit this field.

Value

Provides a list of values to command to the attribute (Normal, Supply Duct Min, Supply Duct Max, Heating Flow, Close All).

Send

Issues the Flow Override command.

Cancel

Closes the dialog box without issuing the command.