Calculate K-Factors Command Dialog Box - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1. Calculate K-Factors Command Dialog Box

Field

Description

Duct Selection

Lists the available ducts to command.

Measured Flow

Use to enter the value measured during the flow override.

Send

Issues the command and calculates the K-Factor values.

Cancel

Closes the dialog box without issuing the command.