System and Device Connections - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Five connection options are available: NxE Passthru, Bluetooth, MAP 4.2+/BACnet Router, ZigBee, and Direct Ethernet. See Connections in the Transfer Operations section for details on these options.