Modules (SP) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
All Simple Plant applications use the core logic listed as follows:

Network Inputs
  • TUNING-RESET: This module is used to reset the tuning parameters to the default values present after the initial application transfer to the device.
Setpoint/Miscellaneous
  • PID Tuning Reset This module forces every output controller to reset the Proportional Band and Integral time of every PID to default values based on current process ID.