Condenser Options (SP) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Condenser Options are:

  • Common Return Temperature: This option monitors the condenser return water temperature.

  • Condenser Flow Sensor: This option measures the condenser flow sensor.

If the No CW Piping (Air-Cooled) node is selected, Condenser Options cannot be selected.