Zone Loop Options (CH) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The options for Zone Loop are:

  • Supply Temperature per Zone: This option adds a temperature sensor to monitor the Zone Loop supply temperature.

  • Return Temperature per Zone: This option adds a temperature sensor to monitor the Zone Loop return temperature.

  • Flow Switch per Zone: This option adds a binary input to monitor the flow in the Zone Loop.

  • Flow Sensor per Zone: This option adds an analog input to monitor the flow in the Zone Loop.