Secondary Hot Water Options (CH) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This section is for general options associated with secondary pumping systems.

The selection options for Secondary Hot Water Options are:

  • Supply Temperature: This option monitors the secondary loop supply temperature.

  • Return Temperature: This option monitors the secondary loop return temperature.

  • Flow Meter: This option monitors the secondary loop flow rate.

  • Building Load Meter: This option monitors the secondary loop BTUs.

If Secondary Variable Speed Hot Water Pumping is not selected, none of these options can be selected.

If Calculate Building Load is selected, Return Temperature and Flow Meter cannot be selected.

If BTU Meter AI is selected, Building Load Meter cannot be selected.

If Calculate Building Load, Loop Supply Water Temp, or Heat Exchangers is selected, Supply Temperature cannot be selected.