General Options (CH) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This section is for general options associated with all systems.

The selection options for General Options are:

  • Loop Differential Pressure Sensor: This option monitors the secondary loop differential pressure.

  • Primary HW Supply Temperature: This option monitors the primary loop supply temperature.

  • Primary HW Return Temperature: This option monitors the primary loop return temperature.

  • Outdoor Air Temperature: This option monitors the outdoor air temperature.

  • Outdoor Air Humidity: This option monitors the outdoor air humidity.

  • Zone Temperature: This option monitors the zone temperature.

  • Mechanical Room Temperature: This option monitors the mechanical room temperature.

If Loop Supply Water Temp or Heat Exchangers is selected, Primary HW Supply Temperature cannot be selected.