Secondary Chill Water Options (CC) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Secondary Chill Water Options are:

  • Supply Temperature: This option monitors the secondary loop supply temperature.

  • Return Temperature: This option monitors the secondary loop return temperature.

  • Flow Meter: This option monitors the secondary loop flow rate.

  • Decouple Temperature: This option monitors the decouple loop temperature.

  • Decouple Flow Meter: This option monitors the decouple loop flow rate.

  • Decouple Flow Direction: This option monitors the decouple loop flow direction.

  • Building Load Meter: This option monitors the secondary loop BTUs.