Primary Cond Water Pumps (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The condenser water systems consist of water cooled chillers, constant or variable speed condenser water pumps, and two-position or proportional isolation valves if the pumps are piped in parallel (common header).