Waterside Economizer (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

For a non-integrated waterside economizer, chilled water is either provided by a chiller or by a heat exchanger, but not simultaneously. Chillers and heat exchangers may either be headered or dedicated (see the following figures). Up to four heat exchangers may be staged up and down to meet the building load. The total number of controlled devices (chillers plus heat exchangers) cannot exceed eight devices.

Figure 1. Waterside Economizer - Primary Headered Chilled Water System

Figure 2. Waterside Economizer - Primary Headered Condenser Water System

Figure 3. Waterside Economizer - Primary Dedicated Chilled Water System

Figure 4. Waterside Economizer - Primary Dedicated Condenser Water System