Condenser Pump Piping Layout (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The condenser water systems consist of water cooled chillers, constant or variable speed condenser water pumps, and two-position or proportional isolation valves if the pumps are piped in parallel (common header).