Parallel Primary CW Pumps (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

In the following figure, the condenser water pumps are connected in a headered or parallel configuration so that any pump may be used with any chiller. The isolation valves are piped to the chillers in a dedicated configuration to prevent water from flowing through an inactive chiller.

Figure 1. Water-Cooled Condenser Headered System