In the following figure, the condenser water pumps are connected in a headered or parallel configuration so that any pump may be used with any chiller. The isolation valves are piped to the chillers in a dedicated configuration to prevent water from flowing through an inactive chiller.
Figure 1. Water-Cooled Condenser Headered System