Dedicated Primary CW Pumps (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

In the following figure, the condenser water pumps are connected in a dedicated configuration. Each condenser water pump is connected to a specific chiller. The condenser water pumps are interlocked to its chiller such that the pump is started before the chiller is enabled.

Figure 1. Water-Cooled Condenser Dedicated System