In the following figure, the condenser water pumps are connected in a dedicated configuration. Each condenser water pump is connected to a specific chiller. The condenser water pumps are interlocked to its chiller such that the pump is started before the chiller is enabled.
Figure 1. Water-Cooled Condenser Dedicated System