Heat Exchangers (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

A waterside economizer provides chilled water to a building using one or more cooling towers and heat exchangers. The Chiller Plant Optimization application supports a non-integrated waterside economizer where chilled water is either provided by a chiller or by a heat exchanger, but both devices do not operate simultaneously.