Cooling System Enable (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection option for Cooling System Enable is OA Cooling Lockout. This input is the outside air temperature setpoint, below which, the system is locked out or disabled. This selection is available only when the Chillers, Condenser Water System node, or both is selected.