Rotate in an Attempt to Balance (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Rotate in an attempt to Balance option allows you to choose your rotation strategy which changes device staging for all devices that have the same COP value based on the selections below.

  • Runtime: This option automatically changes device staging order based on runtime (equal runtime rotation strategy).

  • Start/Stops: This option automatically changes device staging order based on the number of starts and stops (minimize starts and stops rotation strategy).