Constant Speed (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This option changes the default upper optimal percent load to 95% and the lower optimal percent load to 60%.