Optimization Options (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Central Plant Optimization 30 option creates the necessary application integration points. Integration points are setpoints calculated by CPO-30 that the application requires to read and then operate the chiller plant based on these values.