Condenser Options (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Common Return Temperature option monitors the condenser return water temperature. The Condenser Flow Sensor option monitors the condenser flow sensor.

If the No CW Piping (Air-Cooled) node is selected, Condenser Options cannot be selected.