Chiller Options (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Chiller Options are:

Chilled Water Options - Per Chiller

  • Flow Switch: This option monitors the flow switch status of the chiller.

  • Flow Sensor: This option monitors the flow sensor of the chiller.

  • Entering Water Temp: This option monitors the entering (return) water temperature of each chiller.

  • Leaving Water Temp: This option monitors the leaving (supply) water temperature of each chiller.

Condenser Water Options - Per Chiller

  • Flow Switch: This option monitors the flow switch status of the chiller.

  • Flow Sensor: This option monitors the flow sensor of the chiller.

  • Entering Water Temp: This option monitors the entering or return water temperature of each chiller.

  • Leaving Water Temp: This option monitors the leaving or supply water temperature of each chiller.

  • Chiller Alarm(s): This option monitors the general alarm status of the chiller.

  • Chiller Setpoint Adjustment(s): This option generates an AO to each chiller to command the setpoint through the BAS.

  • Chiller Amperage(s): This option monitors the current of each chiller.

  • Primary Supply Temperature: This option monitors the primary supply water temperature.

  • Primary Return Temperature: This option monitors the primary return water temperature.

  • Primary Flow Sensor: This option monitors the primary flow sensor.

  • Refrigerant Monitor Panel Alarm: This option monitors the refrigerant alarm.