Box Flow Test - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

You can only run the Box Flow Test after you transfer the initial application to the controller. The air handling unit's supply fan must be running to implement the Box Flow Test. After completion of the test, the error summary report shows which devices and applications were not installed or set up correctly.

The Box Flow Test consists of two tabs: Setup/Progress and Results. You can use the Box Flow Test Discover feature to discover the test results from the device. After you initiate the Box Flow Test, you can disconnect from the network and return later to collect and review the results.