Table 1 describes the Binary Value object commands. For information about command priorities, see Command Priority Levels.
|
Name |
Description |
|---|---|
|
Operator Override |
Replaces Present Value (Appears as O1) at the Operator Override priority with the value you enter in the command. The override has no effect if a higher priority value is in the Present Value attribute.
Note: This command is available only if the Binary Value is prioritized.
|
|
Operator Override Release |
Releases an Operator Override command.
Note: This command is available only if the Binary Value is prioritized.
|
|
Release |
Releases a specific priority of Present Value (Appears as O1).
Note: This command is available only if the Binary Value is prioritized.
|
|
Release All |
Releases Priorities 3 - 15.
Note: This command is available only if the Binary Value is prioritized.
|
|
State 0 |
Releases command Priorities 9 - 15 and then writes State 1 to Present Value (Appears as O1) at Priority 16.
Note: This command is available only if the Binary Value is prioritized.
|
|
State 1 |
Releases command Priorities 9 - 15 and then writes State 1 to Present Value (Appears as O1) at Priority 16.
Note: This command is available only if the Binary Value is prioritized.
|