Binary Output Object - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The BO object represents a physical binary output. The binary output is always reliable.

You can use the value of this object in logic and to monitor the status of hardware.

For more information on the Binary Output object, see Binary Output Attributes and Binary Output Commands.