Binary Input Object - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The BI object interprets binary signals from hardware and presents them to you as the physical states of the items. For example, a Binary Input can indicate whether a switch is on or off. You can use the state of this object in logic and to monitor the status of hardware. The Binary Input is always reliable.

For more information on the Binary Input object, see Binary Input Attributes and Binary Input Commands.