Humidification (RTU) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
These selections provide the logic to control a humidifier, if present.

The selection options for Humidification are:

  • Staged

    • One Stage

    • Two Stages

    • Three Stages

    • Four Stages

  • Steam Proportional Valve

    • Isolation Valve

  • Modulated Packaged Unit

  • Control Sensor

    • Zone Humidity

      • During Unoccupied Mode

    • Return Air Humidity

  • Discharge Humidity High Limit Control

The During Unoccupied Mode option is applicable only when Scheduled Occupancy is selected.