Sensor(s) for Zones (MADD-MZ) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

These selections allow the user to specify the zone sensors required for each zone.

The selection options for Sensor(s) for Zones are:

  • Temperature

    • Setpoint Adjust

      • Common Setpoint Adjust

      • Warm Cool Adjust

    • Temp Occ Support

  • Humidity

  • CO2 Sensor

The Temp Occ Support option is available only when Scheduled Occupancy is selected.