Number of Zones (MADD-MZ) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This selection specifies the number of zones controlled by the Multizone unit (minimum of two). This selection does not directly load modules, but determines the number of modules loaded for each subsequent Zone Configuration selection. The module for each zone is designated by X (from 1 to the selected number of zones).

  • Two Zones

  • Three Zones

  • Four Zones

  • Five Zones

  • Six Zones

  • Seven Zones

  • Eight Zones