Summer and Winter Compensation Setpoint Shift (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Selecting this option shifts the heating and cooling setpoints to compensate for extreme outdoor air temperatures. This works similar to zone control reset by outdoor air temperature, with a large deadband so the setpoints are not modified while the outdoor air is between 50 and 75 °F.