Occupancy Control (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This section defines how the unit determines occupied status and how it behaves during unoccupied periods. These selections provide the logic for Occupancy Mode Determination.

The Always Occupied option causes the unit to operate in occupied mode at all times.

Note: If any options are selected for separate Occupied and Unoccupied Setpoints or Temporary Occupancy, the Always Occupied option cannot be selected.

The Scheduled Occupancy option adds a network input that causes the unit to cycle between occupied, standby, and unoccupied modes as indicated by the OCC-SCHEDULE. Override Support adds a network input (OCC-OVERRIDE) to allow the user to override the current operating mode. Occupancy Switch adds a binary input connected to an occupancy sensor that changes the current operating mode.