Fan Status (MOA) (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Selecting the option for Fan Status adds a binary input for the minimum outdoor air fan. You may select to restart the minimum outdoor air fan automatically or manually after the loss alarm is cleared. Selecting Manual Restart adds either a BI or Network Input to the system. This input must be commanded to restart the system.