Minimum Outdoor Air Fan and/or Damper (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

These selections provide the logic for a dedicated Minimum Outdoor Air Damper and/or a Minimum Outdoor Air Fan (Injection Fan) with optional damper.

The Fan Status and Damper End Switch are available only for selection if applicable (that is, if fan or damper is selected).