Single Speed Enthalpy Wheel (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This option adds a binary output to control the heat wheel. Single Speed enthalpy wheels rotate at a constant speed when enabled. This configuration can optionally have Modulated Bypass Dampers to control the temperature transfer by bypassing some of the airstream around the wheel.