Pump Status (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This option adds a binary input to monitor the status of the circulation pump. If you select Pump Status, you must also select a Loss of Status Strategy. This strategy can be either Automatic Restart, which continually attempts to restart the heat wheel until the status indicates it is operating correctly, or Manual Restart, which stops the heat wheel until the alarm is reset. The manual restart option offers a choice of using a network input or Unit Reset Switch (BI) to reset the system.